Multiple-Joint Hinges
GN 7237 Stainless Steel-Multiple-joint hinges are installed to be space saving and vandalism-proof inside the housing, they allow a 180° opening angle of the flaps, hatches and doors.
Elongated holes in the hinge mounting brackets and spacer plates make the hinge adjustable on three levels. Like the GN 2370 spacer plates, GN 2376 and GN 2372 threaded plates, are also available as mounting accessories.
Find out more in the current press release or on our webshop.
Click here for the application video!
Back